1/8/2013 12:02 PM | |
Joined: 8/25/2005 Last visit: 3/21/2025 Posts: 1162 Rating:
|
Hello @LAD, SFC51 is supported by the CP 443-5. You have to modify the SCL-ID a little bit if you are using an external DP-Master. Please have a look at the online documentation of the SFC. Think the description there is very detailed. Or have a look ath the following manual: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 Which SCL-ID's did you try to read? Good luck Sabine AttachmentSFC51_from_Manual.pdf (75 Downloads) |
Follow us on