3/26/2012 10:50 AM | |
Joined: 3/18/2008 Last visit: 8/25/2022 Posts: 1750 Rating:
|
Dear jklm, Thanks for your detailed Answer. Now,please answer my following doubts if possible. 1)if Eprom inside the Card is Safe we have no truble means by replacing the card and inserting the Eprom will serve the purpose. 2)but still if i want to take backup from Eprom i need COM535 Software as you said but i dont have it as of now. Here on Siemens Site it is available on Chargable Basis Com535 V4.0. i am using Step5 v7.23+hf2Version. my question is that Com535 V4.0 is compitible with Step5 v7.23+hf2? if yes i can purchase it online. Apart from this is there any license required for Com535 V4.0 separtly? 3)can you provideany Manual or Procedureregarding this Backup procedure? Thanks in advanced. looking forwardfor your earlist reply. |
Last edited by: Amit_86 at: 3/26/2012 11:25 AMVANDE MATARAM..... |
|
3/26/2012 8:02 PM | |
Joined: 7/18/2011 Last visit: 4/13/2023 Posts: 520 Rating:
|
Hi Amit_86, If you're thinking of purchasing software, i suggest that you look for COM143. Using this software you can backup and change software of the CP535 and CP143 which is the successor of the CP535. I use this software together with Step5 V7.20. I'm not surewhetherit is compatible with V7.23. You don't need to install a separate license for this software. Check out this thread as well, about how to get COM143 software. Kind regards, BV |
Last edited by: BeVee at: 3/26/2012 8:12 PMAdded link to COM143 thread. |
|
This contribution was helpful to
1 thankful Users |
3/28/2012 6:00 PM | |
Joined: 3/21/2006 Last visit: 4/12/2023 Posts: 10221 Rating:
|
Hello, http://support.automation.siemens.com/WW/view/en/17264659 Manual is not exist in electronic form. best regards, Hristo Mihalev |
4/18/2012 8:56 AM | |
Joined: 3/18/2008 Last visit: 8/25/2022 Posts: 1750 Rating:
|
Dear All, As discussed, please find attached Procedure for ready reference. Hope this will help since no manual for this backup procedure is available. AttachmentCP535 BACKUP Procedure.zip (129 Downloads) |
VANDE MATARAM..... |
|
This contribution was helpful to
1 thankful Users |
Follow us on