Industry Online Support
Technical Forum
5/26/2009 9:35 PM | |
Joined: 12/5/2006 Last visit: 4/12/2023 Posts: 73 Rating:
|
Hi The 2 CPU's are very similar built in blocks are similar but might be different so make sure you replace any of the built in blocks from the 103 by the built in blocks from 95U, DB1 also might be different. I am not sure if the topic belong to this thread thought it should be belonging to the Step 5 thread. Copy of the 95U manual could be obtained under this link http://support.automation.siemens.com/WW/view/en/1091648 100U under this link http://support.automation.siemens.com/WW/view/en/1091978 If I were you I would convert it to a Step 7 CPU |
6/9/2009 10:21 AM | |
Joined: 8/20/2008 Last visit: 5/10/2022 Posts: 11 Rating:
|
thank you Mr.Safety4ever |
Follow us on