11/18/2011 10:40 AM | |
Joined: 12/1/2006 Last visit: 1/17/2025 Posts: 26 Rating: (0) |
I did a warm reset does not exceed the CPU in RUN mode |
11/18/2011 2:08 PM | |
Joined: 9/28/2005 Last visit: 12/10/2024 Posts: 2957 Rating: (243) |
I would suggest reflash firmware http://support.automation.siemens.com/WW/view/en/38710101 |
Best regards, |
|
10/8/2013 4:32 PM | |
Joined: 6/1/2010 Last visit: 11/6/2024 Posts: 36 Rating: (4) |
It's little bit late but I have the same error on a 1215C and this doesn't work for me. Did you find the solution ? |
7/4/2015 1:19 AM | |
Posts: 3 Rating: (0) |
The firmware 212-1AD30-0XB0_V200.EXE It is valid for cpu 6es7 212-1bd30-0xb0? |
Follow us on