12/31/2023 1:43 PM | |
Joined: 12/28/2016 Last visit: 11/4/2024 Posts: 435 Rating: (52) |
Hello everyone, happy new year I want to use the sample programs below in my project, Ready-for-use example application for SIWAREX WP521 ST / WP522 STbut when I change the cpu and select cpu1515, I get the following error. This problem exists only with cpu 1515 and not with cpu1513. |
Last edited by: Jen_Moderator at: 01/02/2024 09:24:28Link optimized. https://pnap.ir |
|
1/1/2024 3:43 PM | |
Joined: 12/28/2016 Last visit: 11/4/2024 Posts: 435 Rating: (52) |
I found that the problem is with cpu firmware version. The latest version provided for my CPU is 1.8 (6ES7515-2AM00-0AB0) but these functions are only available for FW v2 and above. To compile the program with this cpu, I must have the password of the siwarex function or write a program that can read the weight from the siwarex card. Is there any other solution to solve this problem? Can another function be used? Is there any other program to get data from siwarex card? I hope Santa will help me. Firmware update for CPU 1515-2 PN |
Last edited by: Madadi at: 01/01/2024 15:46:46Last edited by: Jen_Moderator at: 01/02/2024 09:25:35Link optimized. https://pnap.ir |
|
1/3/2024 3:49 PM | |
Joined: 1/4/2007 Last visit: 12/5/2024 Posts: 1153 Rating: (175)
|
Hello Madadi, Now attached the TIA Portal project. Best regards Siwarexi
AttachmentSiwarex_Support_TIA_V16.zip (287 Downloads) |
Follow us on