5/5/2009 11:29 AM | |
Posts: 35 Rating: (0) |
I have successed colect data from one display to cpu300 via CP340 and store it in DB11 as per the attatchment. with two kind of data type (CHAR, same value as on the display, and BYTE). Any one who could help me to use this data and display it (as same value on the display) in WinCC? |
Last edited by: Blue Moderator at: 5/5/2009 9:02 PMSplitted and renamed thread |
|
5/5/2009 11:31 AM | |
Posts: 35 Rating: (0) |
here I attatch with DB11 in CHAR type of data. This is the same value as on the display. |
5/5/2009 2:37 PM | |
Joined: 3/21/2006 Last visit: 1/14/2025 Posts: 10239 Rating: (1182) |
Hello ALU, Look at How can you display an S7 variable of the CHAR type in WinCC? Hope this will helps. Best regards Hriso Mihalev |
Follow us on