1/21/2012 10:06 AM | |
Joined: 3/21/2006 Last visit: 10/4/2024 Posts: 10229 Rating: (1181) |
Hello, 6ES7 312-5BD01 is quite old type CPU. It's successor product is 6ES7312-5BE03-0AB0. That means that it is spare part compatible and will replace the old CPU. If in hardware confuguration you have 5BD01 you can phisically replace it with 5BE03 without to change hardware configuration and to download it. And in this way will work properly. But in case in hardware configuration you have only 5BE03, this will work properly only if you download it in real 5BE03. About update of firmware, I don't think is important in case you are trying somehow 5BD01 to work with TIA 11. Anyway there are instructions Operating System Updates for CPU 312C Best regards, Hristo Mihalev |
This contribution was helpful to2 thankful Users |
2/6/2014 1:37 PM | |
Posts: 2 Rating: (0) |
Dear Daniel, Thanks for your swift reply. The only CPU that I can select as a 312C is a 312-BE03-0AB0 and that does not fitfor the 5BD01. Valère |
Follow us on