Industry Online Support
Technical Forum
9/6/2010 1:30 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328)
|
All S7-300 CPUs can handle 32bit data types, like DWORD, REAL, DINT |
|
|
9/6/2010 7:37 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, This is an old issue. And unfortunately isn't so clear at the moment. Take a look at this thread [?] What is the architecture of S7 CPU's? There have some info... Best regards, Hristo Mihalev |
9/7/2010 12:54 PM | |
Posts: 18 Rating: (0) |
Hi, I think the question is about the size of accumaltor-register. And the answer would be YES. |
10/21/2010 6:59 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
1. S7-317 Infineon TriCore 32-Bit ( www.infineon.com/tricore ) 2. New S7-315 AG10 Infineon IBC16 16 bits 3. Old S7-315 AF03 = Infineon C165 16 bits BR, Hristo Mihalev |
Follow us on