7/25/2015 11:30 AM | |
Posts: 110 Rating: (0) |
Hello Experts, We have a S7 300 PLC ie CPU-315-2D as master and 4 CPU-315-2DP slave plc's.Everything was running perfect till last week and suddenly it went to stop mode. now SYSF indication is constantly red and BUSF is flashing red and CPU mode is stop mode. I have tried to restart the system but same situation. Master CPU is having one more module for SCADA communication which is CP-342-5 which is having no indication now.Please guide me to troubleshoot this problem. Also if i want to access the CPU which version of STEP7 is required and from where I can download this. Regards sandy
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/27/2015 10:44:23 AMNew subject after splitting |
|
7/26/2015 6:35 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello sandy, Please don't post the same question twice! https://support.industry.siemens.com/tf/ww/en/posts/cpu-315-2dp-in-fault/130948/?page=0&pageSize=10 |
This contribution was helpful to1 thankful Users |
7/27/2015 10:45 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on