Industry Online Support
Technical Forum
6/28/2012 6:53 AM | |
Posts: 12 Rating: (1) |
Dear Experts, Good day! I have to replace the old cpu (315-2AF03-0AB0) with (315-2Ah14-0AB0), first i download the new HW configuration the cpu run with no error but when i download the program the cpu stop with sf error (i/o access reading) adrress 352 which is the adrress of FM357 module. Via diagnostic stacks FC2, FC22 cause of error but it is lock and standard program for FM module.. See screen for info.. thanks for the help..<< Best Regards heartbroken
AttachmentFM357.zip (87 Downloads) |
Follow us on