1/22/2011 9:39 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Dear member check if you have OB86 in your CPU. regards AttachmentOB86.pdf (143 Downloads) |
1/23/2011 5:50 PM | |
Posts: 5 Rating: (0) |
sorry for delayed response. Thank you very much hdhosseini. I'll check to see if this solves the problem. |
1/24/2011 8:19 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Perhaps would be useful - Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? Best regards, Hristo Mihalev |
1/27/2011 8:08 PM | |
Posts: 5 Rating: (0) |
well, I added OB86 and I still have the problem. Here is what in Diagnostic Buffer. Any other ideas? |
1/29/2011 8:03 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hi R.GH.B. Check following link for a similar problem: Problem with Profibus
BR |
Follow us on