2/12/2013 11:47 AM | |
Posts: 8 Rating: (0) |
Dear All we have PLC system consists of two CPUs 315-2DP I attache the data of components below as excel file, we have a proplem with PROFIBUS communication network and we havenot any documents or backup program The PLC system used with ABB ACS600 Drives via PROFIBUS Network I tried to upload the program from the CPU with MPI USB Cable but it doesnot response and give (online : no other active partener can be found) I have remove the MMC and take an image and managed to get the Ladder code but unfortnetly I didnt find the hardware configuration so the proplem of communicatio is still running Could any one help me for getting the HW Configuration and network may be this will be helpfulfor our problem Best regards AttachmentPLC Data.zip (173 Downloads) |
2/12/2013 12:00 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, After checking all things mentioned above follow attached document to upload. Make sure you have all GSD files regarding third party slaves installed. Regards, Marcjan Attachmentupload.pdf (287 Downloads) |
Problem solved? |
|
2/12/2013 12:32 PM | |
Posts: 8 Rating: (0) |
Dear UMENCHO Please check below answers for you questions What is the settings in PG/PC Interface? Please check attached Prnt screen PG.PC Interface Does Windows recognize correctly the USB MPI Adapter? Yes it is working well, Please check print screen Detect Network it is only appers when PLC is connected What is the OS and version of Step7? Dear Marcjan I have followed your procedure but when I click View Button the message (Online : No other active partener can be found) and I cant upload any thing Thanks for your help in advance AttachmentPrint Screens.zip (158 Downloads) |
2/12/2013 2:38 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
What is the MLFB number of CPU? |
Follow us on