Industry Online Support
Technical Forum
5/16/2011 3:42 PM | |
Posts: 22 Rating: (0) |
Can i consider that CPU 315 2PN/DP is compatible with software redundancy integrated MPI port? |
5/17/2011 12:52 AM | |
Joined: 1/28/2009 Last visit: 9/9/2024 Posts: 6849 Rating: (1365) |
Check this link for compatible modules: Which modules can you use when implementing software redundancy? and this link for more details: SIMATIC S7-300/S7-400 Software redundancy for SIMATIC S7 check section 7.3 "Hardware configuration for the example with S7 300" regards |
5/17/2011 11:43 AM | |
Posts: 22 Rating: (0) |
Thank hdhosseini. I understand and I achievedthe project hardwareas theattachment. But nowi have 2 cpu(cpu315 2pn/dp) and mpi cable. i want to realize redundancy system with two cpu without IM153-2 andcp345-2as first attachment. i want to test redundancy cpu system. Can i do that? |
Last edited by: ElectricEngineer at: 5/17/2011 11:46 AM |
|
Follow us on