2/14/2012 7:01 AM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Hello GOWDA, Check this for MODBUS TCP requirement (which needs a valid License for S7 OpenModbus/TCP blocks via S7-CPs) * How can you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information? * Communication between SIMATIC S7 and Modicon M340 via Modbus TCP * Wizard for creating connection data for Modbus TCP communication. (Modbus TCP Wizard) Here you find for Open Commuication with 3rd Party - TCP Communication Wizard for creating connection data for open TCP/IP communication (Open Communication Wizard) When your 3rd party device support either TCP Protocol then you don't need to worry on the vendor if it is MOTORALA or others (beware TCP is different and MODBUS TCP is different) |
Last edited by: Ganes10 at: 2/14/2012 8:37 AMAdded the MODBUS TCP FAQ and MODBUS TCP wizard Like it? Rate it! |
|
2/14/2012 8:05 AM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Yes the same CPU can be used for MODBUS TCP as well as TCP communication (with other devices) provided you don't exceed the maximum number of connections for CPU 315-2 PN/DP |
Like it? Rate it! |
|
2/14/2012 1:48 PM | |
Posts: 112 Rating:
|
|
2/14/2012 2:00 PM | |
Joined: 8/31/2010 Last visit: 2/8/2025 Posts: 1524 Rating:
|
Hello GOWDA, SIMATIC HMI KTP 1000 BASIC COLOR PN - 6AV6647-0AF11-3AX0supports MODBUS TCP (Modicon driver) refer this URL under Protocols |
Like it? Rate it! |
|
2/15/2012 4:54 AM | |
Posts: 112 Rating:
|
helle ganes thanks dear................... thanks regards anbugeethan gowda |
Follow us on