Industry Online Support
Technical Forum
5/30/2011 5:10 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
I did see the word crane, reminds me off this : /tf/WW/en/Posts/54520#top So have a good lood at your powerlines and grounding, a crane is mobile so there could be some point where the power or ground can be broken for a short period. Best regards, Marcjan |
Problem solved? |
|
5/30/2011 5:41 PM | |
Posts: 947 Rating: (45) |
In my previus post, I lost - V - 24V. Profibus connector has contacts with +5V and +24 V. When bad montageearthin cablemay close one of these contacts |
Follow us on