4/24/2012 5:34 PM | |
Joined: 8/31/2005 Last visit: 6/14/2024 Posts: 2198 Rating: (326)
|
Yes the one value I looked at was resettet to the orginal value.
I see it like you. When The CPU requires a reset (Urlöschen) all data in RAM ia erased. During the next startup the data from the MMC is loaded again, with the orginal values. PS: With RAM to ROM you can update the values in a DB on the MMC. (see http://support.automation.siemens.com/WW/view/en/15389520, make shure you look in the MMC area of the FAQ) |
|
|
4/24/2012 5:44 PM | |
Posts: 947 Rating: (45) |
Hello! Maybe someone's playful pen instead of the CPU to stop the transfer did reset? This was on my practice. |