6/28/2012 4:49 PM | |
Posts: 19 Rating:
|
I am using cpu 412-3H to communicate with SPPA-T3000.now i have 1 problem, i already add the library in Simatic manager.when i call T3_Link[FB 1110: connection to CM] than CFC close. i do it in a 2nd way but facing the same problem. in FC i call FB 1110, than it is hsowing problem. messages are attached in zip file. please help me out in this issue. Attachment1.zip (72 Downloads) |
6/29/2012 4:34 PM | |
Posts: 19 Rating:
|
how can i make connect CM of SPPA T3000 with S7 in netpro?????? |
Follow us on