7/2/2016 12:11 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308)
|
Hello The Standard Siemens RS232-TTY cable part no is : 6ES5734-1BD20 With this you will possibly also need a 25pin to 9pin serial convertor. There are however many options available , Just Google "SIMATIC S5 RS232-TTY Programming cable " One example : IBH S5-Current loop converter Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
7/2/2016 5:49 PM | |
Posts: 4 Rating: (1) |
There are also USB to TTY converters (Not Siemens). Google PG-USB |
7/15/2016 9:19 AM | |
Posts: 112 Rating: (0) |
Thank you guys I will try and i will write you again. Best regards Adi |
Follow us on