2/1/2011 6:52 AM | |
Joined: 10/7/2005 Last visit: 10/9/2024 Posts: 3024 Rating: (1054)
|
Hello ArmandBaule the simple to answer to "Is SI1 of a 928B the AS511 programmers port?" is: Absolutely YES I hope this helps |
Cheers |
|
2/2/2011 12:47 AM | |
Posts: 19 Rating: (0) |
Thank you very much. I love those kind of short answer
|
This contribution was helpful to1 thankful Users |
2/3/2011 1:07 AM | |
Joined: 10/7/2005 Last visit: 10/9/2024 Posts: 3024 Rating: (1054)
|
No bother dear ArmandBauleand another simple "Yes" answer to your question. The Siemens part number (and link) for it is: 6ES5734-1BD20 Have a look too at the the following two FAQ's: How is the connection between a Windows-based panel and a SIMATIC S5 set up?(it refers to MHI Panels, but is also applicable for PC based WinCC) Why does the online mode not work with the S5-PC converter TTY - RS 232? I hope this helps |
Cheers |
|
2/4/2011 7:49 AM | |
Joined: 10/7/2005 Last visit: 10/9/2024 Posts: 3024 Rating: (1054)
|
Hello ArmandBaule
Simple answer again: NO (you have a 928B CPU which provides the 5V and islisted in THIS FAQ).
No need for any S5 code development, you will get the values directly. I hope this helps |
Cheers |
|
Follow us on