3/3/2011 9:11 AM | |
Joined: 10/7/2005 Last visit: 10/5/2024 Posts: 3024 Rating: (1054)
|
Hello createstars didyouactually configure the IM308C with COM Profibus and if so, what I/O's have you choosen for the link between the IM308C and the S7? Please give us also more details about your proposed system configuration (e.g. I presume your IM308C is the DP Master and theS7 is the DP Slave, but perhaps you plan use DP/DP couplers instead etc.). For now, all I can tell you is that the IM306 DIP switches are only relevant for Digital and Analogue I/O modules as well as add some links to manuals and exampleswhich will hopefullyhelp. ET 200 Distributed I/O System with IM 308-C manual COM PROFIBUS manual PROFIBUS DP Master/slave communication options examples I hope this helps |
Cheers |
|
3/4/2011 1:36 PM | |
Joined: 10/7/2005 Last visit: 10/5/2024 Posts: 3024 Rating: (1054)
|
Hello createstars you say that "In Com ProfibusI have two Im 308C (one master one Slave-S7 Cpu)" which has me a bit confused. I presume you intend to have the IM308C as the DP Master and the S7 CPU as the DP Slave, correct? If so you MUST configure the S7 CPU with the correct GSD file (see HERE for them) as a DP Slave in COM Profibus and there would be only one IM308C in your COM Profibus configuration (representing the DP Master in your 115). Can you please check and verify this and ideally upload your COM PB config file here. As for FB250 & FB251: You are correct, these shouldn't be used in a 944 CPU to read fromAnalogue modules in a DP Slave station of the IM308C (see also HERE for more). Having said that, you said in your first post that the IM308C already existed and that all was working fine before you started to add the S7 CPU to the COM PB configuration, so I doubt that this has anything to do withyour current problem (do you have Analogue I/O's in your existing DP Slave I/O stations? Perhaps they are all in the central or expansion racks in which case the FB250/251 issue won't affect you). I hope this helps |
Cheers |
|
3/9/2011 2:01 AM | |
Posts: 71 Rating: (0) |
Hi Fritz...
I tried to transfer the data using QW in Com profibus and "O" in S5 program. but this would stop the CPU. Could not understand why is that.. I will attach the Pb5 file soon together with the s5 program. Your advice would be much appreciated. Thank you Fritz. Attachmenttesting.zip (173 Downloads) |
3/9/2011 3:00 AM | |
Posts: 71 Rating: (0) |
Hi Fritz, Attachmenttest_OW.zip (145 Downloads) |
3/9/2011 1:25 PM | |
Joined: 10/7/2005 Last visit: 10/5/2024 Posts: 3024 Rating: (1054)
|
Hello createstars can you please clarify which CPU ismeant to be the DP Master and which one the DP Slave? (I thus far presumed that the IM308C is the DP Master, but your your COMPB configuration has no S7 CPU as a DP Slave in it ...) |
Cheers |
|
Follow us on