1/18/2012 8:53 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
Hi Well Yes you can communicate with the Internal DP port of the Two CPU. Please see the attached Link Have fun... |
Jazz |
|
1/18/2012 10:08 AM | |
Joined: 2/6/2009 Last visit: 1/7/2025 Posts: 939 Rating:
|
HI, Sorry, I am not able to get any information from the attached link. Can you please provide another link or Please explain it.
|
_______________________________________________________________ |
|
1/18/2012 10:26 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
Hi Sorry about that, Well see this attached Compedieum of CPU-CPU, The Entry ID:20982954 or the below link will help you. CPU CPU Have fun.... |
Jazz |
|
1/19/2012 7:21 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
Hi well i have done with S7300 System with Ge fanuc System over Profibus DP. You will have to use DP send Recv blocks, But the project file size is very big, basicly what we did was we took the GSD file of the S7300 to the Fanuc system and in our program put the address of our system in the Address input of the Send recive block. See normallly if you want to transfer large volume of data then you will have to go for a profibus CP card (Recomended). See the link1, in that entry ID 20987910 will have the sample code for the same. What are the options for exchanging data between CPUs via MPI/PROFIBUS DP? link1 In your case both the CPU are S7 family.Please see the links below Direct exchange of data between Two CPU S7 family. Link2 Have fun.... |
Last edited by: Tagolover at: 1/19/2012 7:28 PMChange the links Last edited by: Tagolover at: 1/19/2012 7:26 PMLast edited by: Tagolover at: 1/19/2012 7:23 PMJazz |
|
This contribution was helpful to
1 thankful Users |
Follow us on