3/11/2016 7:56 AM | |
Joined: 8/26/2013 Last visit: 7/20/2024 Posts: 35 Rating: (0) |
Sir, My network configuration is as follow: 1. CPU 319-3 PN/DP is connected to TP1500 Comfort panel via PROFINET 2. CPU 319-3 PN/DP is connected to PG via PROFINET 3. CPU 319-3 PN/DP is connected to CANopen-DP gateway via PROFIBUS Problem occurs as follow: When I download the above configuration (including GSD file of gateway) to CPU. CPU goes to RUN mode. But when I switch-ON the power supply of gateway (24V DC), CPU goes back to STOP mode automatically? Screen shots attached. ------------------------------------------------------------------------------------------ AttachmentCAN.zip (178 Downloads) |
Last edited by: Min_Moderator at: 3/11/2016 11:49:05 AMNew subject after splitting |
|
3/11/2016 8:00 AM | |
Joined: 8/26/2013 Last visit: 7/20/2024 Posts: 35 Rating: (0) |
Screen Shot attaced |
3/11/2016 8:01 AM | |
Joined: 8/26/2013 Last visit: 7/20/2024 Posts: 35 Rating: (0) |
Screen Shot attaced |
3/11/2016 8:02 AM | |
Joined: 8/26/2013 Last visit: 7/20/2024 Posts: 35 Rating: (0) |
Screen Shot attaced
AttachmentCAN-DP_Hardware.pdf (202 Downloads) |
Follow us on