5/12/2016 2:12 AM | |
Posts: 15 Rating:
|
The ethernet LED on the 1500 is different. It has only one LED per port. It lights yellow when it has stable connection with IM. Anyway, i'm sure the LED sequence indicates that my PLC can't connect to IM. Could you give me idea what could cause the inconsistent connection? |
5/12/2016 10:36 AM | |
Joined: 8/3/2009 Last visit: 3/21/2025 Posts: 15056 Rating:
|
Hello Keyots I´m sorry here you can see the Meaning of the specialised LEDs of S71500 Bye Murof |
If this Information really helps, you could use the Rate function |
|
5/15/2016 12:02 AM | |
Joined: 9/3/2008 Last visit: 3/20/2025 Posts: 933 Rating:
|
keyots, On both your 1500 and ET200SP go to the ports Advanced options and check that the transmission rate is set to automatic. You can play with setting it to a specific speed, but make sure that they are set identical on both sides. |
Michael |
|
5/17/2016 2:19 AM | |
Posts: 15 Rating:
|
we have resolve the network error by placing an Ethernet switch with the IM. It seems that there is a signal loss using the particular ethernet cable we have when connecting any device to an IM. Thanks to all who sent their ideas. appreciate it alot. |
Follow us on