10/16/2011 11:14 AM | |
Posts: 288 Rating:
|
hello. we have a machine with plc s7-300 cpu315-2dp 315-2af01-0ab0 with mc card 6es7-951-0kf00-0aa0. this cpu also has a battery.what is function of battery? (there is mc card and it doesn't need battery). can you please tell me if data blocks in this cpu are retentive or not? best regards. |
10/16/2011 5:48 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Rechargeable battery: If the CPU is operated without a back-up battery and you only wish to back up the time against power failures on CPUs with a hardware clock, you can insert a rechargeable battery in place of the back-up battery in the back-up battery compartment. In this case only the time is maintained. The RAM and RAM loading memory are not maintained in this case, so a memory card is absolutely essential. A limited number (CPU-specific) of bytes may also be maintained in a data block or by flags, timers and counters. If you insert the back-up battery (buffered CPU mode), the RAM, the RAM loading memory of the CPU and the clock are maintained even if power fails. In this case, all the data blocks and any flags, timers and counters defined in the parameter settings are also maintained. Why does the retentivity behavior of the S7-300 CPUs and C7 devices without MMC (Micro Memory Card) influence the contents of the variables? Best regards, Hristo Mihalev |
We are working on a new user interface with better overview and more relevance.
To explore the new Forum, you can follow the textbox in the right column, which will lead you to the corresponding page in the new Forum. Alternatively, you can start from the main page by following this link:
https://sieportal.siemens.com/en-ww/support/forum
In the coming days, we will update the configuration step by step, so that you are directed to the new Forum by default. The “classic Forum” will remain available for all known functionalities alongside the new one.
We are thrilled to finally share the future of our Forum with you. Thank you for your commitment!
Kind regards,
the Forum Support Team
Follow us on