Industry Online Support
Technical Forum
2/1/2011 8:54 AM | |||||
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Are you using "Siemens" MMC? Take a look at -
|
||||
2/2/2011 1:52 PM | |
Posts: 26 Rating: (1) |
and dont format it with windows |
2/3/2011 5:59 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello If you plug an MMC which was earlier being used in a different CPU model, then also you can have this problem. e.g. if you remove a MMC for CPU 313C and try to use it in CPU 315-2DP, then also similar problem occurs. You need to Format / Reset the MMC in the New CPU. Pl see the link below : http://support.automation.siemens.com/WW/view/en/29801950 Regards Navnag |
There is no such thing as the last bug in a program |
|
Follow us on