6/19/2012 3:23 PM | |
Joined: 8/31/2005 Last visit: 3/13/2025 Posts: 2198 Rating:
|
Make a factory reset at the CPU: https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=29564002699&TopicId=24570788363 Make shure to use the left MPI/DP connector of the CPU! (if there is more than one) Do you use the PC Adapter USB (6ES7972-0CB20-0XX0) or a third party product? The PC Adapter USB gets it's power from the PLC, not from the USB. You must use the short MPI cable (a cable with 4 wire) Is the PC Adapter USB recognized by the PG/PC, when you connect it and switch on the PLC? Did you select "PC Adapter" in PG/PC interface configuration? Did you select "USB" as local port? |
|
|
Follow us on