6/27/2010 5:01 PM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839)
|
Hello ruel, First, I would like to say "Welcome" to Siemens Forum specially this is your first post. Now, my first quick investigation: the problem comes from the profibus network. could you please draw the profibusnetwork of your machine and attachhere. It will help us to tell you where to look and to find a solution. Also, please have a look on this thread Regards. |
Ayman Elotaify |
|
6/27/2010 5:08 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello ruel, Basically if you have some problems with CPU take a look at its Diagnostic buffer. (in Online mode, Ctrl+D). There is possible to find what is wrong there. Take a look also at the following entry tells you which organization blocks do you need for error handling in the S7 program of the CPU: 11499205. best rgeards, Hristo Mihalev |
6/28/2010 9:23 AM | |
Posts: 6 Rating: (0) |
thanks to all your replies, attached is my profibus drawing, please just interconnect them because we dont have a big scanner. i am also attaching my diagnose buffer, as of this writing, all printing units are running but we don't put paint on unit 2 to avoid it from cleaning during idle or change design. this is because when cleaning or change design we need to crawl and that's the time the cpu stopped. hoping for your good advice cause we need to run on 3 colors ruel AttachmentNew.zip (175 Downloads) |
6/28/2010 9:29 AM | |
Posts: 6 Rating: (0) |
sir, this is the continuation of my attached drawing ruel AttachmentNew1.zip (189 Downloads) |
6/29/2010 7:57 AM | |
Posts: 6 Rating: (0) |
hello and good day, Dear UMENCHU, This is the first time we encounter this kind of problem, only on this machine so, regarding on programming organization blocks, we still lacks the knowledge I already downloaded the manual for OB's and Error handling programs and just started reading it. and i think it will take time before i could handle safe inclusions of OB's on our system, i hope you could share us some ideas to resolve our problem. I checked our program we already have OB86, but in our diagnose buffer event no 6 it says ob not found or disabled or cannot be started in the current operating mode. please see my attached diagnose file ruel AttachmentDiagnose.zip (164 Downloads) |
6/29/2010 8:04 AM | |
Posts: 6 Rating: (0) |
Dear mr Ayman, I sent the drawing of my profibus network yesterday, how did you find it? how can i find the problem using the drawing. thank you very much for all you time. ruel |
Follow us on