1/31/2018 5:05 PM | |
Posts: 18 Rating:
|
Hi, Im have a hard time wire my TTL 1x14 (RS422) encoder to my baseunit on my ET200 CPU 1510 system. I have an encoder (6FX2001-2CB02) that i want to connect to my base unit. I have read the manual for my TM-Count module but i cant work it out. In the manual chapter "Wiring" it says wich signal from encoder that goes where if running TTL model. I also have a manual for the encoder but i cant really get the signals to fit.. Anyone who have a wiring diagram between The encoder and the base unit.. //J AttachmentEncoder manual.pdf (76 Downloads) |
1/31/2018 5:56 PM | |
Joined: 7/7/2010 Last visit: 1/27/2023 Posts: 13080 Rating:
|
From what I read in here: TM PosInput 2 is the module for 5V TTL / RS422 encoder signals. Unless you install an encoder signal conditioner that converts from 5V to 24V, you cannot use the TM-Count module.
|
Last edited by: Jen_Moderator at: 2/1/2018 11:19:34 AMInserted right link. science guy |
|
Follow us on