12/2/2015 6:42 AM | |
Posts: 16 Rating:
|
Hello, I have a S7 200 CPU224 which is flashing SF/DIAG and STOP lights. I installed Microwin & SP9 V 4.0.9.25 into win 7 I use the USB - PPI RS485 ( 2013) cable. The cable shows as installed in WIN Device Manager and GREEN TX lights flash when I try to communicate with PLC No RED RX lights. Microwin reports error Communication timed out check port number, network address, baud rate and attached cable. I have tried using the settings as per the manuals (2011) but cannot communicate with the PLC. Help please. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/2/2015 1:26:09 PMNew subject after splitting |
|
Follow us on