5/18/2018 12:29 PM | |
Joined: 8/25/2005 Last visit: 3/21/2025 Posts: 1162 Rating:
|
Hello Kiiza, which CPU are you using exactly? Please send us the MLFB For example checking the technical date of the CPU317-2 PN/DP, 1 MB you get informations about the interfaces that can be used. Via one technical network more than one logical networks could be realized. If you want to read or write data from time to time there would be the option to use "S7 communication" via Put / Get Options. Good luck |
Follow us on