3/8/2018 5:05 PM | |
Joined: 9/27/2006 Last visit: 3/26/2025 Posts: 12344 Rating:
|
Hello Session; Based on this document for your CPU 410-5H, it can be configured as a Profinet IO Controller using its integrated Profinet ports. The CP 443-1 can be used to connect to the plant bus or the AS through TCP/IP or ISO-on-TCP, but cannot be used as a Profinet IO controller. https://support.industry.siemens.com/cs/ww/en/view/96839331 There are various documents in the link based on various versions of PCS 7; the screenshot below is taken from version 9.0. Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
Follow us on