9/26/2008 5:14 PM | |
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating:
|
I think you should try using Structure Tags . Since Structure Tags are same like Arrays with different Elements . First you need to define Structure . Then you can create the Structure tags by selecting the Data Type as Structure . Check this manual for Creating Structure Tag . http://support.automation.siemens.com/WW/view/en/15342782 http://support.automation.siemens.com/WW/view/en/22533646 |
9/26/2008 5:16 PM | |
Posts: 487 Rating:
|
Check thesethree features in WinCC information system.
Some link with info |
Last edited by: JMJ at: 9/26/2008 5:21 PMLast edited by: JMJ at: 9/26/2008 5:21 PM |
|
1/2/2009 2:08 PM | |
Posts: 53 Rating:
|
Solved 4-Use/show in graphic table on runtime [First]: Using SetTag / GetTag functions!, (as recomended by JMJ ) ------------------------------------------------------------------------------------------------- I didn't knew those functions, they are useful! but not a transparent solution when dealing with another data type than byte, the convertion must be done manual... [Second]: to watch data in runtime graphic I use ListBox -------------------------------------------------------------------------------- thanks |
Last edited by: hernan_e at: 1/2/2009 2:12 PMLast edited by: hernan_e at: 1/2/2009 2:11 PM |
|
Follow us on