12/16/2011 11:51 AM | |
Posts: 17 Rating:
|
hi. but in my option i can't acces the {Create GSD file} that a disable thing..
|
12/16/2011 12:17 PM | |
Posts: 376 Rating:
|
Hello, I think you should provide more information about the problem and and your usedhardware. Best regards Azteke0110 |
12/16/2011 1:12 PM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
The source is published at Profinet Card. Now, do not mix 8BA00 with 8BA01. Only in case of the second type of CPU you can generate a GSDML file. Where did you receive this "Transfer"? Make a screenshots of the situation there. Best regards, Hristo MIhalev |
12/16/2011 3:12 PM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
OK, More information about the PROFINET I-device function is available in the system manual "PROFINET, System Description" in the chapter entitled "I Device" in Entry ID 19292127. Best regards, Hristo Mihalev |
Follow us on