8/18/2015 10:55 AM | |
Posts: 15 Rating: (0) |
This has got to be a very simple task but I somehow managed to fail at it. I have the switch (see attachment) from the library. It is a switch that is either turned on bright (and stays bright) or turned off dark (and stays dark). My problem is with how to indicate it with a text that when it is at On and Off states. I also tried to imitate this with a button and played around with the Events and Animations but failed again. What is the simplest way of handling this? Thanks! AttachmentPictures.zip (387 Downloads) |
Last edited by: Min_Moderator at: 8/18/2015 11:30:33 AMAdd attachment |
|
8/19/2015 3:16 PM | |
Posts: 15 Rating: (0) |
Is there anyway to have the text (input field in this scenario) over the switch without it interrupting the clicking action? |
Follow us on