9/8/2020 1:05 PM | |
Posts: 2 Rating:
|
hello, I need help in creating another instance of the same project running on another PC even if it doesn't have the capability of creating a database. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/08/2020 14:38:51New subject after splitting |
|
9/10/2020 12:59 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello X-maarno I do not understand your usecase, please can you describe it in a different way? DO you want to start a second instance of a RUntime on the same PC? or do you want to load the Advanced RT into more thatn one PCs? It wold be good if you write an example or something that we can understand better? Thanks and Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on