7/7/2022 9:56 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello Siemens_Repair_Man with build in functionality it is not possible to get a csv file with a column for each tagname. The Basic structure of the log files is fixed by the system and you cannot change it. https://support.industry.siemens.com/cs/de/en/view/109798671/124435008139 You could do your own logging with VB Script, then you can define how the structure should be, but if you use fast logging cycles then it could be that single entries in the textfile would be too slow. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on