1/17/2017 8:13 PM | |
Posts: 11 Rating: (1) |
Dear Experts, We are trying to interface CU250S-2 with SEW Motor Encoder of type AG7W ( see attached Datasheet and Connection Details) . We are using an SMC20 Module for this type of encoder. However, We are getting fault 31150 on the drive. Please help to resolve the issue. We have connected A/A*/B/B*/Clock/Clock*/Data/Data* from Encoder to X520 apart from Power and GND. Also, in the encoder details, we have entered encoder type as SSI encoder with sin/cos, Binary, Multiturn, Single turn resolution- 8192, Multiturn Resolution-65536, Pulses/rev-2048,Pulse freq-200kHz as per the encoder datasheet Attachment3 Connection SEW Encoder.pdf (152 Downloads) |
1/17/2017 8:15 PM | |
Posts: 11 Rating: (1) |
Datasheet for the Encoder is also attached for reference
Attachment3 Encoder Datasheet.pdf (136 Downloads) |
2/8/2018 9:02 AM | |
Posts: 1 Rating: (0) |
Hi, could you please share your application of SEW encoder? AG7W is not SSI format, try AG7Y |