12/23/2016 6:23 AM | |
Posts: 1 Rating:
|
I have updated my current obsolated controller CU320 to CU320-2 in which new components like CIM, AOP, TM, IPD were changed. After simulation all the old chasis firmware were upgraded to new one. Load trials taken found healthy. After running of more than 50 hrs drive tripped on the F05064 Fault. Please find the topology image which is configured in CU. Please go through the topology and suggest whether it is correct or not. Please note that we have two motor modules and two BLM for our 2MVA drive unit. In this conversion we have not change the chasis as mentioned earlier all were upgraded with the firmware only. Pl. answer as soon as possible. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/24/2016 3:32:53 AMNew subject after splitting |
|
Follow us on