11/26/2015 10:23 AM | |
Joined: 5/12/2006 Last visit: 2/7/2023 Posts: 21227 Rating:
|
Hello, please refer capter 13.14 in the sinamics S function manual https://support.industry.siemens.com/cs/ww/en/view/99686093 1) you can enter the key in starter if you are online or in the parameter 9920 2) steps described in the linked manual 3) if licence is correct installed no Warning Message is active and the RDY LED of the system should be Green (if no error is present ;) ) Regards Christoph |
12/12/2015 5:24 PM | |
Joined: 5/12/2006 Last visit: 2/7/2023 Posts: 21227 Rating:
|
Hello, from the function manual Capter 13.14 (Page 888) "The "Performance" option (order number: 6SL3074-0AA01-0AA0) is required as of the 4th If you have 4 Axises then there is no other solution then buy a licene, or use only 3 Axises.
Christoph |
Follow us on