8/16/2011 6:53 PM | |
Posts: 13 Rating: (0) |
Thanks Alan, the linked app did the trick. |
Last edited by: Bob2246 at: 8/16/2011 6:53 PM |
|
8/22/2011 4:00 AM | |
Posts: 133 Rating: (13) |
Please be advised. The factory setting of the internal Ethernet interface X127 of the Control Unit is 169.254.11.22. |
12/15/2021 2:43 PM | |
Joined: 4/28/2009 Last visit: 9/16/2024 Posts: 347 Rating: (43) |
Hello, if you have access to this forum, you can also download Starter, it is for free. You can change IP address of X150 port of your drive in Starter under Commisioning interface -> IP interface configuration. Or, if you don't want download Starter, you can use Proneta software, it can be also used for setting IP address and device name. With regards, Martin |
Follow us on