8/8/2013 3:51 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986)
|
Hello, first you must create a PROFINET IO-System on the SIMOTION! TODO. Select the Slot X150 -> right Mousclick -> insert IO-System at this point you must create a Ethernet or connect a available Ethernet Now you should have a PROFINET System on the SIMOTION. Select the CU320 in the HWcatalog and drag and drop trho the created IO-System. A step by step ist described in the communication manual of SIMOTION Regards Christoph |