Industry Online Support
Technical Forum
7/28/2011 7:53 PM | |
Posts: 11 Rating: (0) |
Hi I`m new at Automation, two fast questions: A) [snip] ... B) I have a problem with HW configuration, I have my unit outside the CPU (315-2dp) configuration and when I try to open the it form STARTER it says: HW conf. cannot be opened the Device s12_cu320_2_dp is not part of step7 station or the HW is unknown, have the GSD from here http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=49217480&caller=view, my MENAGER is V5.4 + sp5 + hf4... splitted from: cu320_cf_card |
Last edited by: CS Moderator at: 7/31/2011 9:37 AMnew subject after splitting Last edited by: ziro_sub at: 7/28/2011 10:56 PMLast edited by: ziro_sub at: 7/28/2011 9:01 PM |
|
Follow us on