8/13/2020 11:13 PM | |
Posts: 1 Rating:
|
The same thing happened to me, the CU320 kept restarting, until just staying in the restart state. Also the Line module was showing RDY: Orange continuously DC Link: OFF This is not a possibility in the manual so I did not know what it meant. We first made the power supply 23.8V to 26V per siemens tech support recommendations. This did not work, we also replaced the 24V power supply. Did not work. Tech support mentioned that the other possibility is a bad CU320 and we would need a new one. This was all caused by something getting wound up in the motors. Update to come...
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 08/14/2020 10:05:11New subject after splitting |
|
Follow us on