8/16/2017 8:10 AM | |
Joined: 5/12/2006 Last visit: 7/1/2022 Posts: 20610 Rating:
|
Hello, https://support.industry.siemens.com/cs/ww/en/view/109480497 If you use a C/D Type which is spare part for a existing one then you can use it with the OLD CU320. The new Types (3 ones) you can only be used with CU320-2 V4.7 HF17 or above. But node that the connectors for motor are complete changed so you must use new cables or a adapter to connect the old one!
Christoph |
Last edited by: ChristophD at: 8/16/2017 8:11:38 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on