11/26/2014 9:14 PM | |
Posts: 5225 Rating: (1192) |
Hi there. You can use any number in any order. However check what is the biggest number you can use for FCs. I think the 128 refers to the maximum count you can create and not the maximum number name you can use. According to my source you can create 1024 counts and 7999 as the biggest number name. But this might be for higher CPU versions. (see PDF) Greetings. w AttachmentEXTRACT_s7300_parameter_manual.pdf (66 Downloads) |
11/27/2014 7:31 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, With these older CPU's you can't number the FC above the limit given in the Tech. details. See i.e. /tf/WW/en/Posts/114754 Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to2 thankful Users |
Follow us on