3/17/2016 12:37 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi saran, I guess so. Look at this manual: SIMATIC Fault-tolerant systems S7-400H
hope this helps, regards, |
FCK WAR! |
|
3/18/2016 9:02 AM | |
Joined: 10/7/2005 Last visit: 3/24/2025 Posts: 3042 Rating:
|
Sorry, but using redundant IM153-4 PN in one ETM200 station is not (yet) possible (one day it will/should be as a Profinet standard exist for this). Using a single IM153-4 PN based I/O station with an S7-400H is possible though as this IM supports system redundancy, have a look too at System Redundancy with IM 153-4 PN for more on this. I suggest you grab also a copy of Configuration Examples for S7-400H with PROFINET SIMATIC S7-400H as of
V6.0 for everything else you want to know on this subject. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
3/22/2016 10:36 AM | |
Posts: 2 Rating:
|
Hi, Thanks for the information Regarding Profinet IO Communication, whether IM level Ring Network is possible? Attached system configuration is possible to provide IM level redundancy? Regards, Saran AttachmentSystem Configuration.pdf (218 Downloads) |
Follow us on