10/7/2016 8:52 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Please have a look: Why does my SIMATIC S7-300 CPU go into STOP with error 16#4548 ... |
This contribution was helpful to2 thankful Users |
10/13/2016 1:00 PM | |
Joined: 5/12/2006 Last visit: 9/17/2024 Posts: 22358 Rating: (3010) |
Hello, can you provide the complete diagostic buffer and not ony the Stop message? Regards Christoph |
10/14/2016 12:24 PM | |
Joined: 1/28/2010 Last visit: 7/26/2024 Posts: 66 Rating: (0) |
Hello Mr. ChristophD, Please find the attached diagnostic buffer txt file for your reference. I am attaching the program also in next post. I don't find multiple attachment option for this post. Regards Shankar AttachmentDiagnose_315PnDp.txt (258 Downloads) |
Last edited by: shankar78 at: 10/14/2016 12:27:56 PM |
|
10/14/2016 12:29 PM | |
Joined: 1/28/2010 Last visit: 7/26/2024 Posts: 66 Rating: (0) |
program with 315 pndp
Attachment315pnDp.zip (272 Downloads) |
10/14/2016 12:30 PM | |
Joined: 1/28/2010 Last visit: 7/26/2024 Posts: 66 Rating: (0) |
program with old CPU 315-1AF03
AttachmentUpload_315_1AF03.zip (190 Downloads) |
10/20/2016 12:52 PM | |
Joined: 1/28/2010 Last visit: 7/26/2024 Posts: 66 Rating: (0) |
Nobody has the solution |
10/29/2016 11:20 AM | |
Joined: 1/28/2010 Last visit: 7/26/2024 Posts: 66 Rating: (0) |
Dear Mr. Duris, We have kept all the settings similar to OLD CPU. Only found additional option in new CPU ie "Size of process image input area" & "Size of process image Output area". Default value is 128. Attached snap for your reference But when I have searched the manual in old CPU it was also 128 but it was not settable. I need urgent help in this regard. AttachmentHW_Comparison.pdf (313 Downloads) |
Follow us on