10/25/2021 9:58 AM | |
Joined: 8/17/2008 Last visit: 3/20/2024 Posts: 6 Rating: (1) |
Hi! I also have the same problem. Currently TIA 17. Does not find any accessible nodes. But I don't think it's a problem of the TIA portal. The same problem that no device can be found also occurred with STEP 7. However, via STEP 7 I will connect to the device without any problems. The PING device also works. All available devices are shown to me using the PRONETA software. Other third-party network scanning software will also find the device. But in TIA 17 I am not able to connect to the device because no device is found. Turning off antivirus doesn't help. Connection without a router, by wire directly to the device. Is there a setting in WIN 10 that needs to be changed? (Reinstalling TIA didn't help :) ------------------------------------------------------------------------------------------ |
Last edited by: MikePAD at: 10/25/2021 10:04:20Last edited by: The Helping Hand at: 10/25/2021 11:26:06New subject after splitting |
|
10/25/2021 1:46 PM | |
Joined: 7/9/2015 Last visit: 5/24/2024 Posts: 3848 Rating: (562)
|
Hi you can try to reinitialize your interfaces - please check the following FAQ: How do you generally parameterize the PG/PC interface and how do you ensure that the device driver can be selected and is visible?Regards, Towome |
Last edited by: Towome at: 10/25/2021 13:50:26
|
|
10/25/2021 7:08 PM | |
Joined: 3/2/2016 Last visit: 5/8/2024 Posts: 72 Rating: (14) |
Hi MikePAD, Have you try running TIA as admin? Is you O.S compatible with TIA Portal V17 installation? |
10/26/2021 11:16 AM | |
Joined: 7/9/2015 Last visit: 5/24/2024 Posts: 3848 Rating: (562)
|
Hi, I would do a service request at Siemens support. |
|
|
10/29/2021 12:03 PM | |
Joined: 8/17/2008 Last visit: 3/20/2024 Posts: 6 Rating: (1) |
So in the end I solved the problem by reinstalling WinCC flexible.... |
10/6/2022 1:50 AM | |
Joined: 1/16/2015 Last visit: 5/21/2024 Posts: 46 Rating: (1) |
i am facing the same problem now, i tried that and it didn't work. |