5/10/2019 12:19 PM | |
Joined: 6/30/2014 Last visit: 8/28/2024 Posts: 463 Rating: (89)
|
Hello, I have heard that it is not possible to add a own "User Control" to the user interface of a query. But the other way round will work: you can create an own user control, add the Top Query Browser or Query Browser to it and use the control in COMOS. As „Extension object“ for a query you can enter the name of a DLL as so called Query-Extender. A class inside this module implementing the interface IExtended can be used for Data-handling of the query. Search for “IExtended” in the COMOS documentation (chapter IExtended in Class Documentation ivbQuery). If a class also implements the interface IQBrowserEvents you can act on the defined events. Search for “IQBrowserEvents” in the COMOS documentation (chapter IQBrowserEvents in Class Documentation ivbQuery). In case you need some support, please have a look into this document: https://support.industry.siemens.com/cs/ww/en/view/109486136 All the COMOS ressources can be found here, on the COMOS Overview page: https://support.industry.siemens.com/cs/ww/en/view/109739837 All the very best, SuperPippo |
Last edited by: Jen_Moderator at: 05/10/2019 12:54:39Optimized links. |
|
This contribution was helpful to1 thankful Users |
Follow us on