8/26/2019 6:19 PM | |
Joined: 9/27/2006 Last visit: 3/19/2025 Posts: 12344 Rating:
|
Heĺlo Arthur; Siemens is a huge conglomerate, and predicting how their offerings in a very small part of their markets will evolve is very difficult. Especially if like us you are looking in from the outside. What is known about Siemens and Profibus: Siemens contributed to the development of Profibus standards and equipment (as defined butthe German government), and implemented an early version, known as Sinec L2, with their S5 PLCs. When Profibus was launched officially, Siemens became one of their early sponsors, introducing it as the main distributed I/O network for their S7-300 and S7- 400 PLCs upon their inauguration. From Wikipedia, the free encyclopedia PROFIBUS Protocol Information PROFIBUS (Process Field Bus) is a standard for fieldbus communication in automation technology and was first promoted in 1989 by BMBF (German department of education and research) and then used by Siemens. It should not be confused with the PROFINET standard for Industrial Ethernet.PROFIBUS is openly published as part of IEC 61158. https://new.siemens.com/global/en/products/automation/industrial-communication/profibus.html With the introduction of the newer S7-1200 and S7-1500 models, the emphasis is being placed on Profinet for distributed stations. But Profibus is always offered as an option using extra CPs, probably due to the high number of installed Orofibus nodes in industry and machinery. Siemens has a history of maintaining support for existing equipment over a long period, even at it ceases to be manufactured. And the market shows no sign of abandoning Profibus for IOs, drives, PLC networking...So I do not think you will have to worry anytime soon about losing access to Profibus on your Siemens controllers. Just my 2 cents... Hope this helps, |
Last edited by: dchartier at: 08/28/2019 16:08:33 |
|
This contribution was helpful to
2 thankful Users |
Follow us on